CIMPLICITY Configuration REST API Web Service
CIMPLICITY Configuration REST API Web Service / All Operations Resource Group / /projects/{projectId}/users (Get)
Get/projects/{projectId}/users
Description
returns a list of users in a project that satisfy the filter criteria
Parameters
NameDescriptionData Type
the id of the project to look instring
number of records to skip for paginationinteger (int32)
maximum number of records to returninteger (int32)
provides a wild card string to filter users by their UserID.string
provides a wild card string to filter users using their corresponding RoleID.string
200 Response

The response body is of type UsersGetResponse.

The collection of users that satisfy the query.

Overview

UsersGetResponse
The results of the users get query.
Users : Array[CimUser]
AuthenticationType : CimUserType
Enable : boolean
PasswordExpiresInDays : number
Password : string
Resources : Array[string]
RoleID : string
UserID : string
UserName : string
Fault Responses
FaultDescription
This fault returns a response body of type ProblemDetails.
project with the given id is not registered on the system
See Also